2024-06-17 5:16 PM
Solved! Go to Solution.
2024-06-21 12:33 PM
TIM20 is configured to have its trigger as OC1. If ADC has its trigger set to TIM 20 OC1, it will not sample. If ADC has its trigger set to TIM20 trigger, then things work as normal. TIM20 OC1 and trigger should be the same...but I guess not.
2024-06-21 12:33 PM
TIM20 is configured to have its trigger as OC1. If ADC has its trigger set to TIM 20 OC1, it will not sample. If ADC has its trigger set to TIM20 trigger, then things work as normal. TIM20 OC1 and trigger should be the same...but I guess not.