2008-07-11 4:00 AM
ADC in debug mode
2011-05-17 3:39 AM
Is it possible to stop the ADC continuous conversion in debug mode?
I configured the ADC1 in continuous mode with EOC interrupt flag activated, so when I try to debug the application the ADC1_2_IRQHandler is continuously called and the other code isn't executed. Is there a method to stop also the ADC clock like DBGMCU_Config(DBGMCU_IWDG_STOP,ENABLE) functions?2011-05-17 3:39 AM
Hi utelettronico,
According to my little knowldge about the MCU, it is not possible to stop an IP while debugging: so you cannot stop an ADC configured in continuous mode while debugging (I hope that I'm not talking nonsense :-] ) Try to work with polling, put a test on the EOC flag in your code, without activating the interrupt: while(1) { if(ADC_EOC_SET) { ADC1_2_IRQHandle } your treatment here /* it must be a short code to not exceed the ADC period */ } B.R. sword2011-05-17 3:39 AM
Thank you sword_82,
your solution work perfectly! Thank you very much utelettronico