2023-09-13 11:54 AM
Using HAL_ADCEx_Calibration_Start() to calibrate the ADC. This function always returns HAL_ERROR.
Debugging shows its failing after it collects the 8 samples and attempting to disable the ADC is timing out. (ie. if ((HAL_GetTick() - tickstart) > ADC_DISABLE_TIMEOUT) is TRUE.)
Using CubeMX to generate drivers. CubeMX version 6.8.1
Note: ADC conversion are working IF I don't calibrate.
Thanks for your help.
Solved! Go to Solution.
2024-03-31 3:01 AM
Why it is not correct in the HAL library ?
2024-04-01 4:02 PM
Hi @DAlbe.3 ,
I was trying to reproduce the problem using your code on a STM32G0B1 Nucleo, but for me, it worked without the delay.
Can you please post the code with context, i.e. what exactly are clock settings, and what is before this piece of code, so that the problem can be reproduced?
Thanks,
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.