cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F373CCT6 SDADC initializing problem

Ada
Associate

Hi, I'm trying to initialize SDADC of my STM32F373CCT6 chip based on the Standard Peripherial Library. The program can be compiled with no errors but doesn't work after I uploaded it to the chip. I used a LED program to test it and found that the initializing function got stucked at the statement of waiting for calibration to complete. I used a self designed board. The intializing function and the main function of my program, as well as the schematic diagram of my board is attached. I'm a STM32 beginner and haved been troubled by this issue for days, I sincerely hope to get your help. Thank you so much!

1 REPLY 1
TDK
Super User

If you're a beginner, I recommend using HAL instead of the SPL. It is better in every way. CubeMX will generate the initialization code for you.

If you feel a post has answered your question, please click "Accept as Solution".