2022-11-15 07:52 AM
Modified the BLE_Throughput example to use indication characteristics instead of the notification.
I also set the interval to 1 second for debugging purposes because I saw that only 1 IND is read by the client per connection interval.
I see that SendData function is called frequently.
The characteristics is only sent 1/s to the client.
The aci_gatt_update_char_value returns 0x0C.
What is this error code?
How could I push more "messages" to the IND characteristic?
2022-11-16 04:45 AM
Do I understand the BLE spec correct that IND requires at least 1 connection interval of "round trip" to be ACKed therefore 1 IND/interval is allowed?
0x0C means already updated?