2013-01-02 8:55 PM
Hi,
I have an STM32F4 discovery board and I want to access SD card via SPI. The reason why I want to access Sd card via SPI is that the breakout module that I have has an SPI interface. I have looked on the internet but have only found examples which are accessing SD card using the SDIO interface. Is there any way that I can get some example code for reading SD card via SPI or some wiring alternative to convert the SPI interface to SDIO interface so that I can use the available examples. This is the module that I have http://www.aliexpress.com/store/product/SD-Card-Reader-Module-for-Arduino-ARM-Read-and-Write-Free-shipping/316774_526750081.html Regards #duplicate-thread2013-01-03 2:30 AM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Accessing%20SD%20card%20via%20SPI%203604¤tviews=6]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Accessing%20SD%20card%20via%20SPI%203604¤tviews=6