cancel
Showing results for 
Search instead for 
Did you mean: 

AC6 Firmware install fails

Ingo Wolf
Associate II
Posted on October 31, 2017 at 23:25

Hi group,

I have installed the AC6 Plugins in eclipse oxygen and try to create a test project for F3 Discovery.

I've choosen Standard Peripheral Library and pressed 'Download Firmware'.

There is something 32 MB downloaded and then installed but that seems to fail with

'Not able to establish connection to remote host !'  but I think the message is wrong, something else fails.

I've tried another directory in the settings also, no luck.

Any ideas?

2 REPLIES 2
Ingo Wolf
Associate II
Posted on November 01, 2017 at 00:26

I now have installed the whole Ac6 IDE with the installer and has the same issue.

http://openstm32.org/tiki-view_forum_thread.php?forumId=7&comments_parentId=5967&threadId=5969&thread_sort_mode=commentDate_asc#threadId=5969

 
Imen.D
ST Employee
Posted on November 02, 2017 at 12:37

Hello

ingo.wolf

,

Thank your for report this issue.This is reported internally to the appropriate team andunder investigation.

As recommended by

http://openstmorg/user13331

in the openstm32 Community, please use SW4STM32 V2.2 or use HAL libraries.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen