2016-08-04 8:04 PM
Dear all,
I am using stm32L151VD.I got an application which needs to change the RTC wakeup counter reload value in run time. My original wake up period is 1/16s. And then I use the code below to change the wake up period to 10s. /* Allow access to RTC */ PWR_RTCAccessCmd(ENABLE); RTC_WakeUpCmd(DISABLE); RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div16); RTC_SetWakeUpCounter(0x5000 - 1); /* wake-up at 10s*/ RTC_ClearFlag(RTC_FLAG_WUTF); EXTI_ClearITPendingBit(EXTI_Line20); /* Enable Wakeup Counter */ RTC_WakeUpCmd(ENABLE); /* Disallow access to RTC */ PWR_RTCAccessCmd(DISABLE);Although the wakeup time changed eventually, but it will trigger one interrupt (old 1/16s interrupt )before the 10s reload value apply. Any idea how to eliminate that unwanted interrupt? #stm32-rtc