2020-09-02 7:50 AM
I have a bootloader + 1 wire serial uploader code
because of space restrictions it uses LL_ libraries for initialization.
We have different hardware designs,
when using PA2 as IO pin it works !
when using PB4 as IO it does not !
The main program uses HAL_libraries
there both pins work as expected.
are there differences in Initialization between GPIOA and GPIOB
when using LL_ ?
what am I missing ?????
this is the initialization section
void systemGpioInit(void) {
  LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
  LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
  LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOB);
 
  GPIO_InitStruct.Pin = INPUT_PIN;
  GPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;
  GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
  LL_GPIO_Init(INPUT_GPIO, &GPIO_InitStruct);
}
					
				
			
			
				
			
			
				
			
			
			
			
			
			
		2020-09-02 11:40 AM
There's no difference in initialization. Gotta be a bug somewhere, doesn't appear to be in the small section of code you posted. Keep checking.
Examine the GPIO registers.
2020-09-02 10:41 PM
@TDK
How can that be ?
when using PA2
the 1 wire read routine recognizes the bootloader init string correctly
(0x0d 0x42 0x4c 0x48 0x65 0x6c 0x69 0xf4 0x7d)
when using PB4 i get
(0x34 0x08 0x30 0x20 0x94 0xb0 0xa4 0xd0 0xf4)
This is the read routine :
void fourWayGetChar() {
  fourWayConfigReceive();
  fourWayRxByte = 0;
 
  while (!(INPUT_GPIO->IDR & INPUT_PIN)) {
    // wait for rx to go high
  }
 
  while ((INPUT_GPIO->IDR & INPUT_PIN)) {
    // wait for rx to go low
    if (TIM2->CNT > 250 && fourWayCharReceived) {
      return;
    }
  }
  // wait to get the center of bit time
  delayMicroseconds(FOUR_WAY_BIT_TIME_HALF);
 
  uint8_t bitIndex = 0;
  while (bitIndex < 8) {
    delayMicroseconds(FOUR_WAY_BIT_TIME);
    fourWayRxByte = fourWayRxByte | ((( INPUT_GPIO->IDR & INPUT_PIN)) >> FOUR_WAY_SHIFT_AMOUNT) << bitIndex;
    bitIndex++;
  }
  // wait till the stop bit time begins
  delayMicroseconds(FOUR_WAY_BIT_TIME_HALF);
  fourWayCharReceived = true;
}
 
void fourWayConfigReceive() {
  LL_GPIO_SetPinMode(INPUT_GPIO, INPUT_PIN, LL_GPIO_MODE_INPUT);
}
 
void fourWayConfigTransmit() {
  LL_GPIO_SetPinMode(INPUT_GPIO, INPUT_PIN, LL_GPIO_MODE_OUTPUT);
}
 
void delayMicroseconds(uint32_t micros) {
  TIM2->CNT = 0;
  while (TIM2->CNT < micros) {
    // wait
  }
}
					
				
			
			
				
			
			
				
			
			
			
			
			
			
		2020-09-03 3:11 AM
A small update:
I took a closer look at the received data in binary
I use 19200baud 8N1
PB4 (bad) , PA2 (good) , PBX = PB4 >>2
PB4 1011 0000 1010 0100 1101 0000 1111 0100
PA2 0110 1100 0110 1001 1111 0100 0111 1101
PBX xx10 1100 0010 1001 0011 0100 0011 1101
It seems that the data is delayed approximate 100µs and some "Hi" bits do not get read.
Like some sort of capacitance pull down lowpass filter is active on the input.
2020-09-03 7:30 AM
Looks like the external pullup could be too weak, or missing. Or the pin is connected to something else on the board affecting the signal.
2020-09-03 9:55 AM
@TDK
No.
This is definitely a LL_ library problem
I will begin debugging GPIO and RCC registers, to see the differences !
br, adrian