2010-09-20 09:01 PM
3.5' 320x240 TFT with Touch & LCD controller SSD2119 supporting 8/16-bit 8080, SPI or Parallel RGB interface
2011-05-17 05:08 AM
I used the SSD1963 to drive a 480x272 on my design. It works OK, the limitation is the FSMC requiring four cycles per write, thus restricting ultimate graphics speed.
And the documentation is not great. Chris.2011-05-17 05:08 AM
Hello, Chris, If you need any help, please feel free to contact with me. E-mail:
mailto:jacky_sheng@kitronix.com