cancel
Showing results for 
Search instead for 
Did you mean: 

16-bit audio with STM32F429

Goguey.Pascal
Associate II
Posted on January 16, 2015 at 06:08

Hello!

I need to have 16-bit audio, 4 channels (at least) input with STM32. Has anybody

developed something like this?

I found many ADCs on the net, but how to get ADC data without spending too much

time on interrupts? I mean: if I have one interrupt for every sample at 48 kHz, the

processor might become quite busy. The ideal case would be an ADC with some

internal buffer that I can fetch once it's full.

Internal ADC would be ideal, but 16-bit devices are only in some F3 devices running

at 72 MHz, and since I need some graphics performance as well, so 429 is almost a must.

Any hint is welcome.

Thanks,

Pascal

#16-bit-adc
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on January 16, 2015 at 09:02

> Any hint is welcome.

Two hints for you: I2S, DMA.

JW