cancel
Showing results for 
Search instead for 
Did you mean: 

STUSB4761-

PVala.1
Associate II

Hi,

We are designing the Android accessory and we would like to use STUSB4761 in our application.

STUSB4761 can source power and become device by receiving DR_swap from the sinking device.

Also we would like to put our accessory to continues in device and source to power the android phone than we can use this chip ?

In STUSB4761 there are two pins opto drv and FB that will work if I will connect 5V input

( using required components )coming from the adapter ?

0 REPLIES 0