cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-MCSDK V.6.3.1 has no BLDC motor selection

NamZC14
Associate

 

Hi,

I am currently working on a research and development project for a Dual Inverter Air Conditioner, where I need to run a BLDC motor for the compressor in the outdoor unit.

I have installed the X-CUBE-MCSDK version 6.3.1 and started exploring its features. However, I noticed that in the motor selection section, there are only 11 motor options, all of which are for PMSM motors.

I am a bit confused as to whether I can operate a BLDC motor using this software and if any of the available PMSM motor options can be adapted to run a BLDC motor. Could you please advise on how to proceed with this, or if there are any necessary modifications I should make?

Thank you for your support.




1 REPLY 1
Gael A
ST Employee

Hello NamZC14,

Did you have a look at this post ?

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.