cancel
Showing results for 
Search instead for 
Did you mean: 

WorkBench not working correctly!

trgyada
Associate II

When i generate file in workbench, get error. WorkBench not found cubemx but i have cubemx 5.3.0 version. Photo in below.0690X00000AA6WDQA1.png

6 REPLIES 6
Ozone
Lead III

I have neither (Cube/Workbench).

Perhaps you have installed Cube into a non-standard folder, and need to manually tweek it in the workbench settings ?

trgyada
Associate II

Thank you for your comment. But not like that problem, i use MC_WorkShop_1.5.exe for installation. I didnt change any folder.

I mean, did the MC-Workshop installer do a Cube installation as well ?

Worth to check if everything is right.

Perhaps your PC has some language/country specifics ST did never test, and result in a broken installation.

Would not be the first time.

Yes solved, thank you for your information. This issue be based on languange settings. Changed to english and solved.

Ozone
Lead III

ST software is for the brave and fearless tinkerer ...

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards