cancel
Showing results for 
Search instead for 
Did you mean: 

Why No FreeRTOS available with H563ZI in MC workbench

PQ
Associate II

In MCSDK 6.2.0, it says "Selected hardware boards do not support this feature". 

In MCSDK 6.3.2, nothing.

Why?

Without this, it generates MC code using systick, and if adding FreeRTOS with CubeMX, I have to merge the systick handlers for FreeRTOS and MC and some other works. The change is "volatile" when generate code with CubeMX again.

I'm heavily rely on CubeMX, so what's the solution?

0 REPLIES 0