2019-05-08 3:11 AM
We have STM3240G-Eval and STEVAL-IHM028V2 boards.
we are trying to run the bldc motor of (24 pole-pairs,1.4KW) with motor profiler (MC-SDK 5.3.3) and we also tried with another motor (8 pole-pairs , 30W) .
the profiler isn't able to calculate Rs, Ls and Ke Values. but after 20% to 25% of profiling it is showing "The measurement is talking too much time".
we also decrease current and max. speed but the result are same.
2021-06-14 11:49 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards