2021-11-30 05:23 AM
I use Schematic diagram of "EVSPIN32F0251S1" in my design with Hall Sensor and I use all its configuration for my board :
and I used a below BLDC motor :
power:300W
current:10.5A
voltage :36V
speed:3000 RPM
but I do not have any move in my motor
and output phase U and V is:
I have no Ls and Rs and B_emf about my motor
2021-12-20 11:02 PM
Dear @HAMIDREZA
Sorry for the late answer.
Do you have still this problem to solve?
And just in case, if not, do not hesitate to share the final solution you found. Thanks by advance.
Best regards