2020-11-13 07:21 PM
2020-11-19 01:11 AM
Dear @Fchun.1
I edited a little bit your message title.
Best regards
Laurent Ca...
2020-12-12 08:45 AM
Hi,
I think so because the "reference current" is set by setting the voltage across the comparator. The voltage can be formed using a DAC or PWM. This is not a PWM output, but a PWM input...
2021-02-21 09:16 PM
The IMH07M1's driver IC integrates an "uncommitted" comparator. This comparator can be used for controlling the current by shutting down the PWM pulse-by-pulse.
In motor control application the 2 input given to the comparator are :
So, the comparator will give output to shutdown the PWM pulse if current drawn by motor is more than set value.
You can find detailed information in this application notes