cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I find the example FW project of P-NUCLEO-IHM002?

OChen.1
Associate II

Hi!

My P-NUCLEO-IHM002 arrived few days ago. Now I'm trying to understand how its FW code works.

I'm wondering where I can find the example FW project (preferably a STM32CubeIDE project) that build the default executable bin file inside that STM32F302R8? (That is, maybe the source project file that builds STM32CubeExpansion_SPN7_V1.1.0/Projects/Multi/Examples/MotorControl/Binary/STM32F302R8-Nucleo/X-CUBE-SPN7.bin?)

Regards,

Oliver

1 ACCEPTED SOLUTION

Accepted Solutions
Claire O.
ST Employee

Dear OChen,

I will advise you to use the example located inside the XCUBE_MCSDK: https://www.st.com/en/embedded-software/x-cube-mcsdk.html

The legacy version (5.4.8) includes P-NUCLEO-IHM002 support.

I don't advise the STM32CubeExpansion_SPN7_V1.1.0 that is not maintained any more...

Thanks and best regards,

Claire

View solution in original post

4 REPLIES 4
Claire O.
ST Employee

Dear OChen,

I will advise you to use the example located inside the XCUBE_MCSDK: https://www.st.com/en/embedded-software/x-cube-mcsdk.html

The legacy version (5.4.8) includes P-NUCLEO-IHM002 support.

I don't advise the STM32CubeExpansion_SPN7_V1.1.0 that is not maintained any more...

Thanks and best regards,

Claire

Dear Clair,

First thank you for your prompt reply and advice.

Under the following path of MC_SDK_5.4.8:

  C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.4.8\Projects\P-NUCLEO-IHM001\Demonstration\

there are two sample projects look like what I need:

  PotentiometerAdvance\

  Potentiometer\

If they are, I'm wondering which one I should use?

Regards,

Oliver

Both should be fine for you. You can start with Potentiometer that is the simplest.

Best regards,

Claire

OK, I see. I'll start from the easier one.

Thanks again for your advice.

I wish you a wonderful day!