cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-F302R8 : USB drivers installed, jumpers configuration done, but when I connect to the PC the LED LD2 remains OFF, LD1 blinks in red, LD3 red, and the PC don't see the device (No ST-link detected). Otherwise the board is working and the motor spins.

MKOTE.1
Associate II
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MKOTE.1
Associate II

Dear Laurent,

The problem was in the USB cable that transmitted power but no data.

I changed the cable and it is working now.

Btw, it would be a good idea to provide the cable with the board!

Best regards,

Mohamad

View solution in original post

6 REPLIES 6
Claire O.
ST Employee

Hello MKOTE.1,

Can you please specify which SW you are using?

Thanks and best regards,

Claire

MKOTE.1
Associate II

Hello Claire,

I tried with Motor Profiler, STM32 ST-LINK Utility, ST MC Workbench, EWARM, etc.

This is the first time I use the board, I've never seen the LED LD2 blinking.

Thanks,

Mohamad

Hello Claire,

I tried with Motor Profiler, STM32 ST-LINK Utility, ST MC Workbench, EWARM, etc.

This is the first time I use the board, I've never seen the LED LD2 blinking.

Thanks,

Mohamad

MKOTE.1
Associate II

Any other suggestions? I need to be able to program the board.

Laurent Ca...
Lead II

Dear @MKOTE.1​ 

Do you have still this problem to solve?

If not, do not hesitate to share the final solution you found.

Best regards

Laurent Ca...

MKOTE.1
Associate II

Dear Laurent,

The problem was in the USB cable that transmitted power but no data.

I changed the cable and it is working now.

Btw, it would be a good idea to provide the cable with the board!

Best regards,

Mohamad