cancel
Showing results for 
Search instead for 
Did you mean: 

What is the RevUpCtrl_Handle_t used for?

llm
Associate III

I can not understand the component of RUC? Can you explain what is the RevUpCtrl_Handle_t used for? when should I use it?

1 REPLY 1
GMA
ST Employee

Dear llm,

Firstly, we would like to sincerely apologize for the delay in replying to your post.
Rev-Up control component is used to start motor with the Field Oriented Control technique.
Since WB6.1.0 version, from WB interface you have access to WB documentation by clicking About>Documentations>Documentation.
On components tab, you have a "FOC Rev-Up Control component" description chapter with a link on RevUpCtrl_Handle_t structure description.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA