2019-06-18 06:05 PM
If anyone has an example of how they communicated with the STEVAL -SPIN3201 motor controller that they can share, I would greatly appreciate it. The chip used on the board is a STSPIN32F0, and it communicates on USART configured as an interrupt. I have the workbench software working with it just fine, but I'd like to communicate with it using a serial port. Thank you for any help you can offer.
2021-06-22 01:29 AM
"STM32 Motor Control" topic added.
Best regards