cancel
Showing results for 
Search instead for 
Did you mean: 

Use a resolver with Motor control

Doublesets
Associate II

Hello,

I am working with Motor Control Workbench 6.4.1 for a project using Nucleo-G431Rb X-NUCLEO IHM08M1 and a PMSM motor. The position feedback is given by a motor resolver.

I read sin e cos values and calc the rotor position correctly.

If I generate a sensorless firmware all work but the issue is that I cannot find the option for a resolver in the Motor Control Workbench, only Hall sensors or Quadrature Encoder. Is there any way to go past this restriction for this use case, either through hardware or software ?

Any assistance is much appreciated.

Thank you

2 REPLIES 2
GMA
ST Employee

Hello @Doublesets,

Thank you for your interest in our products.
As mentioned, only Hall sensors or quadrature encoders are supported in the current MCSDK version implementation.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
ThisIsDursun
Associate II

We had the same issue and decided to use a zero-crossing detector circuit to convert the sine-cosine waveforms to the quadrature waveforms.

Although it adds some delay, but it still works.

Regards