2011-12-28 6:28 PM
[Resolved]: When the Over-current protection disabling network check box is clicked on the (Power Stage - Over Current Protection) page the port and pin values can then be changed.
----------------------------------------------------------------------------------------------- I am unable to change the port and pin for the Over current Protection Disable in Motor control workbench. All the enables for this are set properly. I can edit the output files and change the pin but not in the MCWB application. Is this a bug or am I missing something? Photo included shows option greyed out.2012-01-02 1:05 AM
Ciao Ericc
I read that you have already resolved the issue but, to be clear, I want to explain better it for all other people. The over current protection disabling feature is intended to be used together with the on over voltage action ''Turn on low side switches''. So to enable are required the three steps below 1) Enable the Over-current protection disabling network in the power stage2021-06-27 11:09 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards