cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to Control Low-Speed Operation

Danu_Park
Associate II

Hello,

I am experiencing an issue with low-speed RPM control in a project created using MC Workbench. After setting a specific RPM in ST Motor Pilot and pressing Start, the motor does not initially rotate. When I set the RPM to -2000 and then suddenly change it to around 3000~4000, the motor starts rotating. Once the motor is running, it can be controlled properly in the 3000~5000 RPM range, but it cannot be controlled in the 0~3000 RPM range.

I have attached the specifications for the motor I am using. It is the 024 model, and I am using a 1024-pulse encoder. The board I am using is the EVLSPIN32G4-ACT board.

Changing the PI coefficients does not improve the issue.

 

Thank you.

 
Danu
0 REPLIES 0