2021-12-01 07:09 AM
I have SVSPIN32F0251S1 board and a BLDC motor without sensors that i am trying to get to spin but the example for this board inculded in the motor control workbench does not work(and gives a lots of error even before it can be compiled).
And if i try to make a custom project based on the board in the motor control workbench i can connect to the motor pilot software and get some data and get the motor to click but the software always gives errors and it seems to be something wrong with the current reading(if protection is enabled it gives over current fault and if not the power meter shows 65000W).
Has anyone got this board to work with the example software?
2021-12-20 11:04 PM
Dear @MRask.1
Sorry for the late answer.
Do you have still this problem to solve?
And just in case, if not, do not hesitate to share the final solution you found. Thanks by advance.
Best regards
2021-12-22 12:42 AM
I still have the same problem