2024-11-19 7:06 AM
Hello,
While I did tests with my motor control STEVAL-IHM028V2, I made a mistake to schort-circuit the three-phase output ! Then, I smelled a burning smell and no voltage is given in the three-phase output . When I checked the bottom face of the device, I noticed that some resistors (R74, R75 and R69) are burned (see attached images). Also, the W7 and W8 jumpers are short-cicuited. How could I fix this issue ?
N.B. The schematic of the STEVAL-IHM028V2 is attached.
Cordially
Tarek
Solved! Go to Solution.
2024-11-27 12:20 AM
Hello @Tarek_ben,
You can try to replace all of these components (resistors/jumper).
Set a conservative limitation current on your external DC supply.
Verify that DC voltages are correctly generated on the board.
Monitor the current consumption when relaunching test.
2024-11-21 4:42 AM
Any answer about this ?
2024-11-26 7:51 AM
Hello @Tarek_ben,
On your IHM028V2.jpg picture, nothing seems to be burned...
2024-11-26 8:02 AM
Thank you for the answer.
If you zoom in on the resistances R74, R75 and R69, you can see a black line in the middle of these resistances.
2024-11-27 12:20 AM
Hello @Tarek_ben,
You can try to replace all of these components (resistors/jumper).
Set a conservative limitation current on your external DC supply.
Verify that DC voltages are correctly generated on the board.
Monitor the current consumption when relaunching test.
2024-11-28 6:59 AM
Thank you.