2023-10-31 2:36 PM - edited 2023-11-01 2:08 AM
Picture 1 SDK 6
picture 2 SDK 5.4.8
Hello,
I want to drive a BLDC motor via IHM16M1 with the newly purchased nucleo-stm32f103rb board. But the control cart is not here. Old version SDKs are also available as XML files(f103rb). SDK 6 introduced the .json extension. And it can't generate code in older SDK versions.
Can anyone help me drive the motor?
Solved! Go to Solution.
2023-11-02 12:41 AM - edited 2023-11-02 5:16 AM
Hello Osman_Faruk_Avcı,
Unfortunately, the STM32F103 MCU is no longer supported by our MCSDK. If you want to work on the NUCLEO-F103RB board, you need to use MCSDK version 5.4.8 which is the last version supporting F1 MCUs.
2023-10-31 2:40 PM
what stm32f103 card ?
2023-10-31 2:45 PM
Stm32f103rb board
2023-10-31 2:48 PM - edited 2023-10-31 2:50 PM
nucleo or what ?
show pic...name of cpu is not enough.
2023-10-31 2:53 PM
Yes nucleo.
2023-11-02 12:41 AM - edited 2023-11-02 5:16 AM
Hello Osman_Faruk_Avcı,
Unfortunately, the STM32F103 MCU is no longer supported by our MCSDK. If you want to work on the NUCLEO-F103RB board, you need to use MCSDK version 5.4.8 which is the last version supporting F1 MCUs.