cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 motor control support?

GBuke.1
Associate

Anyone know when/if the H7 series will have more motor control support? The F series can't do what I need and only 1 chip (which has an eval board) can be used in MCWB but it is extremely limited.

6 REPLIES 6
Claire O.
ST Employee

​Dear GBuke,

We have right now, some code example for the H7 linked to the MCSDK (but as it is code example, you cannot modify it with MC workbench).

Is that helping you or do you need full H7 support?

Thanks and best regards,

Claire

kswarm
Associate II

Hi Claire,

The example given for the H7 is only for the the dual-core uC H745ZI. Any idea of when is the H7 single core going to be supported?

Thanks,

E

Laurent Ca...
Lead II

Dear @kswarm​ , dear @GBuke.1​ 

Do you have still this problem to solve?

Best regards

Laurent Ca...

kswarm
Associate II

Hi Laurent, @Laurent Ca...​ 

as you can see I never got answered the question I did, it would be nice if you could give us more information about it.

Thanks a lot!

E

Claire O.
ST Employee

Dear @kswarm (Community Member)​,

We have no plan to add STM32H7 single core in our MCSDK, sorry...

I guess the easiest solution for you will be to use an STM32F7 project and modify it.

Thanks and best regards,

Claire

VKost.2
Associate II

Do plan to support any of H7? If yes, when?