cancel
Showing results for 
Search instead for 
Did you mean: 

STIB1560DM2T-LZ - VccH and VccL current rating

PiPPiP
Associate II

Hello,

How do I determine the power rating for Vcc input to STIB1560DM2T-LZ.

Regards,

PiPPiP

3 REPLIES 3
GMA
ST Employee

Hello @PiPPiP,

You can refer to the STEVAL-IPMM15B board, which is based on the STIB1560DM2T-L SLLIMM™ product.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
PiPPiP
Associate II

Yep, have looked at that at length - is there an easy answer?  1A perhaps?

PiPPiP
Associate II

Or failing an easy answer, can you help me work out what the rating should be from the figures in the quoted dev board (I spent the weekend looking and could not work it out).

Thanks

PiPPiP