2018-09-21 5:51 AM
I generate a STEVAL-SPIN3202 project (Keil MDK) by ST Motor Control Workbench V5.2. But it doesn't work. The motor was BR2804-1700kv-1 sensor less motor from P-NUCLEO-IHM001 KIT.
Motor didn't really spin. I got FOC duration faults when I started motor in Monitor page of Motor Workbench. Communication was OK without problem.
I have other two ST evaluation KIT which are P-NUCLEO-IHM001 and STEVAL-ESC001V1. Both of them work perfectly with ST Motor Control Workbench V5.2 and BR2804-1700kv-1.
My questions are:
Thanks,
Ian
2021-06-22 2:15 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards