2020-12-17 10:09 AM
STEVAL-SPIN3201
After looking at the schematic i can see that there is a second MCU to 'control' the STSPIN32F0.
This second MCU has a STLINK connector for programming. My question is ; Is it possible to program the STSPIN32F0 directly and not have to use a second MCU. I am looking to program the STSPIN directly and not use any 'ready made' firmware. Is this possible with this evaluation board ? With this set up i dont see any way to utilize the hardware features of the integrated MCU within the STSPIN.
Solved! Go to Solution.
2020-12-17 10:06 PM
Hello
This eval board contains a STLink(stm32cbt6) that means STSPIN32F0 can be programmed and debuged by USB cable with your custom firmware and without any extra hardware tool.
The connector you mention is for programing STLink (UM 2154)
2020-12-17 10:06 PM
Hello
This eval board contains a STLink(stm32cbt6) that means STSPIN32F0 can be programmed and debuged by USB cable with your custom firmware and without any extra hardware tool.
The connector you mention is for programing STLink (UM 2154)
2020-12-18 5:36 AM
Thank you !