2019-06-06 7:35 AM
Hello!
I'm trying to work with steval-spin3201 board, i have AMETEC minijammer bldc motor with three hall sensors on board, ST Motor Control Workbench with Atolic True studio. First i tried sensor-less control and it's works fine with some tuning. But i can't rotate motor with hall sensors connected, motor stuck in one position and don't moving. What i did: in ST Motor workbench i selected Hall sensor instead of sensor-less, connected three hall sensor to board with 5V_USB power. I checked signal on hall sensors: it changes when motor rotating, so they alive. Can you suggest something? Thanks!
Some update: i managed to rotate motor with the hall sensors, i have to change "Sensors displacement" to 60 deg (because of hardware placement of sensors), but i can't understand what is "Placement electrical angle" mean?
Regards,
Roman.
2019-08-07 1:18 AM
Dear Roman,
I encounter the same problem with you, may i know which software version you are using? According the STM Motor library V4.3, you need to manually set up hall sensor. Refer to manual below, page 89 onwards.
2019-08-07 2:02 AM
Yes, thank you! That was a decision for me
2021-06-22 1:32 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards