cancel
Showing results for 
Search instead for 
Did you mean: 

Error in code which is generated by St motor workbench

NK.13
Associate II

i have generated code from motor control workbench and when i build this code the error came as,

region `FLASH' overflowed by 18000 bytes StSpin_Hall_24_07 C/C++ Problem

StSpin_Hall_24_07.elf section `.text' will not fit in region `FLASH' StSpin_Hall_24_07 C/C++ Problem

i tried for optimised the code code then the there is no error but motor is not working well.......

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards