cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-CTM009V1 for ACIM FOC Control

Ymtr
Associate
  • Hi everyone,

I’d like to learn more about FOC algorithms and eventually design my own motor driver. For this purpose, I’m planning to use the STEVAL-CTM009V1 to drive a pump or traction motor similar to those used in forklifts.

In general, forklifts with around 2-ton lifting capacity are based on a 48V architecture, and I already have access to such a system for testing.

My main question is:

Can I drive an ACIM (induction motor) with the STEVAL-CTM009V1? I’m not fully sure about its capabilities in this regard. If it is possible, are there any reference projects or examples that I can follow?

Also, when using Motor Control Workbench, which control board would you recommend pairing with the STEVAL-CTM009V1?

I should also mention that I’m already familiar with FOC concepts and have experience designing forklifts and telehandlers, but this will be my first time designing a motor driver from scratch, so I’d really appreciate any guidance or best practices.

Thanks in advance for your help!

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @Ymtr,

You have to adapt the provided examples to your use case.
Examples are based on NUCLEO-G431RB. Refer to STM32 MCU Developer Zone page for MCU/board selection tools.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

3 REPLIES 3
GMA
ST Employee

Hello @Ymtr,

You can refer to STM32 MC SDK AC Induction Motor link. This document is linked to the examples provided in the MCSDK6.3.2 suite, and the STEVAL-IHM023V3 power board is used.

In MCSDK6.4.2 suite, the examples are based on the STEVAL-IPM10B/STEVAL-IPM15B power boards.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

So, just to confirm — does this mean I can adapt these examples to drive an encoder-based ACIM motor using the STEVAL-CTM009V1?

I also have one more question:
Do you have any recommended control board to use together with the STEVAL-CTM009V1?

Thanks in advance for your support

GMA
ST Employee

Hello @Ymtr,

You have to adapt the provided examples to your use case.
Examples are based on NUCLEO-G431RB. Refer to STM32 MCU Developer Zone page for MCU/board selection tools.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA