2021-05-11 6:20 AM
I try to configure current sensing pin map in ST Motor Control Workbench. But there seems a problem during combo box selection. I am able to select one of A0/A1/A2 for Phase U, whereas these items are not available for Phase V selection combo box. Check please the screenshots. This can be a software bug ? Any comment ?
2021-05-11 10:09 AM
I recognized that this problem exists when the board is selected as custom, when I changed to STEVAL-ESC001V1 inside stmcx xml file, I can see the missing combo box items. These xml nodes are under <system type="common">.
======= Problem ================
<board_name>Custom</board_name>
<original_board_name>Custom</original_board_name>
======= No problem ================
<board_name>STEVAL-ESC001V1</board_name>
<original_board_name>STEVAL-ESC001V1</original_board_name>