2018-04-17 8:25 AM
What are the use of the Power Measurement classes in the ST MC FOC lib v4.3?
From the confidential distribution the following classes are part of MC Library module:
MotorPowerMeasurementClass
PQD_MotorPowerMeasurementClass
There is no info on this in UM1053.
#power-measurement2021-06-27 9:07 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards