cancel
Showing results for 
Search instead for 
Did you mean: 

smt32f103 Lost code of circuit B G431 ESC1

Nguyenhuuphuchieu
Associate

Mạch B G431 ESC1, tôi vô tình xóa mã bên trong stm32f103 nên giờ tôi không thể kết nối với mạch, ai đó có thể giúp tôi với mã tệp hex để tôi có thể tải lại trên stm32f103 không. Cảm ơn

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Nguyenhuuphuchieu, to the community!

The STM32F103 on the B-G431B-ESC1 acts as ST-LINK/V2-1, which cannot be deleted accidentally, but only intentionally. However, the firmware of all of the ST-LINK is not available for official download, so you would have to buy a new B-G431B-ESC1.

By the way: since the entire forum speaks English, of course I write in English, even though it's not my native language.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.