cancel
Showing results for 
Search instead for 
Did you mean: 

Sampling 3 phase current with only 1 ADC

MMila.3
Associate

Hello,

In motor control pack P-NUCLEO-IHM001, microcontroller is STM32F302R8 which has only 1 ADC.

The motor drive has option to use 3 current shunts.

By analyzing the datasheet, ADC does not have multiple sample & hold circuits.

So, how would it be possible to sample 3 phase current with this mcu?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
cedric H
ST Employee

Hello,

We sample only two phases and reconstruct the third one. We select the two phases to sample according to the electrical position of the rotor.

With the configuration with one ADC, the two sampling are executed in a row.

Regards

Cedric

View solution in original post

3 REPLIES 3
Laurent Ca...
Lead II

Adding of "Motor Control Hardware" topic. 

Best regards

cedric H
ST Employee

Hello,

We sample only two phases and reconstruct the third one. We select the two phases to sample according to the electrical position of the rotor.

With the configuration with one ADC, the two sampling are executed in a row.

Regards

Cedric

Thank You for the answer. Now I understand that it's ok to do 2 samples 1 after another.