cancel
Showing results for 
Search instead for 
Did you mean: 

Request for 3D CAD Models of EVSPIN32G4-DUAL Evaluation Board

pelino
Associate III

Hi,

Could you please let me know where I can download the 3D CAD model (e.g., STEP/IGES) of the EVSPIN32G4-DUAL evaluation board?

Thank you!

Best regards

Pelino

1 ACCEPTED SOLUTION

Accepted Solutions

3D CAD files for this board are not available. What is available has already been pointed out. If that is not sufficient, you will either need to create a 3D model yourself or adjust your project to proceed without it.

Sometimes there are user-created models for more popular boards, but I don't see anything for this one.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

9 REPLIES 9
GMA
ST Employee

Hello @pelino,

All available CAD resources are provided here.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
pelino
Associate III

Only Gerber files are available here; there is no 3D file.

pelino
Associate III

Only Gerber files are available here; there is no 3D file.

Hello @pelino,

This CAD page provides the available resources for this board.
Gerber-to-STEP converter tools are available, but not from STMicroelectronics.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

Why do you feel the need for 3D files?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I am planning to design a product that will operate with this board, and in order to proceed with the design, I will need the 3D file.

Note that ST boards are for evaluation/development only - not for incorporating into a product.

See the Terms of Use.

via: https://www.st.com/en/evaluation-tools/evspin32g4-dual.html#documentation

 

PS:

This is also stated in the User Manual:

AndrewNeil_0-1769004856818.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I are not planning to use it for industrial purposes; it is intended for demonstration purposes only.
Is it possible to provide the 3D drawings?

3D CAD files for this board are not available. What is available has already been pointed out. If that is not sufficient, you will either need to create a 3D model yourself or adjust your project to proceed without it.

Sometimes there are user-created models for more popular boards, but I don't see anything for this one.

If you feel a post has answered your question, please click "Accept as Solution".