Skip to main content
Associate III
Jan 12, 2026 10:56 PM UTC
Solved

Request for 3D CAD Models of EVSPIN32G4-DUAL Evaluation Board

Hi,

Could you please let me know where I can download the 3D CAD model (e.g., STEP/IGES) of the EVSPIN32G4-DUAL evaluation board?

Thank you!

Best regards

Pelino

TDK
TDKBest answer
Jan 22, 2026 12:02 AM UTC

3D CAD files for this board are not available. What is available has already been pointed out. If that is not sufficient, you will either need to create a 3D model yourself or adjust your project to proceed without it.

Sometimes there are user-created models for more popular boards, but I don't see anything for this one.

"If you feel a post has answered your question, please click ""Accept as Solution""."

9 replies

GMA
ST Technical Moderator
Jan 19, 2026 3:00 PM UTC

Hello @pelino,

All available CAD resources are provided here.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
pelinoAuthor
Associate III
Jan 19, 2026 10:38 PM UTC

Only Gerber files are available here; there is no 3D file.

Andrew Neil
Super User
Jan 21, 2026 2:04 PM UTC

Note that ST boards are for evaluation/development only - not for incorporating into a product.

See the Terms of Use.

via: https://www.st.com/en/evaluation-tools/evspin32g4-dual.html#documentation

 

PS:

This is also stated in the User Manual:

AndrewNeil_0-1769004856818.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
pelinoAuthor
Associate III
Jan 19, 2026 10:37 PM UTC

Only Gerber files are available here; there is no 3D file.