2014-01-22 02:51 PM
Hello,
Does anyone know
where I
can find the Source Files for the''MC_FOC_Methods_lib.lib'' and ''MC_State_Observer_lib.lib''
?There
are
parts of the open
source code
in
the
library files
,where you can not
look
inside.
Can someone
send
the source
files
for
me?
2014-01-23 06:46 AM
Ciao Hans,
Both MC_FOC_Methods and MC_State_Observer are protected parts of the motor control code. It can be released for free just after signing an appropriate ''Non-disclosure agreement (NDA)'' with ST. If you require it please contact your nearest ST office. Ciao Gigi2014-03-24 10:19 PM
Dear Gigi,
I am using a
STM32103VBT6 and STM32 PMSM FOC based BLDC program.
It works very well when it
drive a 16 inch hub BLDC motor(56 poles), but it has problems when driving a 14 inch (46 poles) hub BLDC motor whose speed is less than 60RPM.
It is unsmooth at low speed. The motor will produce large torque ripple
when hall sernsor
.
It also works well when
run
ning
at high speed.(>5km/h)
Can you tell me how to adjust
the
program to
14 inch hub BLDC
motor?
ThanksAlenEmail: xmgatech@gmail.com2014-03-31 01:16 AM
Ciao
URL :
/92e3f1c8
2021-06-28 03:03 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards