2018-09-11 08:10 AM
Hello,
In folder ESC_STM32_FOC_FW we have working solution for STEVAL-ESC001V1 including PPM input control.
However, after identifying the motor parameters , the generated new project located in ESC_STMCWB_prj folder does not include files found in ESC_STM32_FOC_FW required by PPM mode control. As I understood from pdf files, with older 4.3.0 version ,the generated project suppose to be in ESC_STM32_FOC_FW but with actual 5.2.0 version, new project is created and the only way to control the motor is by the GUI interface provided.
So how to compile the project to include the new identified motor parameters as well as ESC (PPM read) function ?
Any help is appreciated.
Regards,
Sergiu
2021-06-22 02:16 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards