2016-03-24 10:42 AM
Hi, i have some problems to build a project for P-Nucleo IHM001_singledrive kit !
When i open the project it said me that some options are broken and when i build the project (after use workbench tool to configure the motor) i have this error :startup_stm32f302.s Error[438]: This instruction is not available in the selected cpu/core C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Common\Libraries\CMSIS\CMSIS_2_x\Device\ST\STM32F30x\Source\Templates\iar\startup_stm32f302.s 173Error while running Assembler
arm_biquad_cascade_df2T_f32.c
Fatal Error[Pe1696]: cannot open source file ''arm_math.h'' C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Common\Libraries\CMSIS\CMSIS_2_x\DSP_Lib\Source\FilteringFunctions\arm_biquad_cascade_df2T_f32.c 41 Can you help please ?2016-03-29 8:59 AM
2016-04-01 5:33 AM
Ciao
Sorry for the delay... yes, updating the IAR solves the issue. Ciao Gigi2021-06-17 12:49 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards