cancel
Showing results for 
Search instead for 
Did you mean: 

CubeProgrammer does not. acknowledge ST-Link v hardwar

XKSteve
Visitor

After much too much time searching and following advice from for the most part, outdated forum posts I have been unable to resolve my issue with win 11.

I have a windows 11 machine (Microsoft Surface) up to date as of 28th January 26.

ST Link Utility installed and woking

StCubeProgrammer 2.21.0 and working (apart from not seeing the STLink v2.0 hardware).

Both installed as Administrator.

Cube Programmer however refuses to acknowledge the STLink v2 when connected even though the driver reports it is working and indeed it shows up in Device Manager. I did try reinstalling and the other common resolve I see is to switch to Shared Enabled in the right hand panel.

The odd bit is it just works on my Mac M2 Tahoma without any issues and displays the correct serial number

I would like to get it working on my Surface laptop as well as all my programming is normally done on that machine (XGecu T48).

Here are some screen shots.

Any suggestions as to what to do to get CubeProgrmmer to see the ST-Link v2.0 hardware on Windows 11.

1 REPLY 1
TDK
Super User

Looks connected to me. It reports a target voltage. Can’t do that without it being detected. Connect button can be clicked.

Fake ST links often have a bogus serial number but may otherwise work okay.

If you feel a post has answered your question, please click "Accept as Solution".