PFC doesn't work on STEVAL-IHM034V2 board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-08-25 2:12 AM
Hi,
i'm using the a STEVAL-IHM034V2 board for evaluation (PFC + FOC PMSM).
I imported the project in ST Workbench 4.3. Generated files and compiled with IAR is OK. Then board is programmed.
The motor starts but the PFC doesn't work.
I verified in the file Drive parameters.h that the PFC is enabled : the following line is present
#define PFC_ENABLED /* #define PFC_ENABLED to enable the PFC */
so the PFC should be enabled.
With serial communication i get the PFC_Status = 0x10
(Id 0x4D)
and the PFC Flags = 0x00100010(Id 0x4E)
which means that the AC frequency is not in the correct range. The AC Mains Frequency is read as 0 with the serial communication (Id 0x51).The pin for AC Mains is B4 (Timer 3 channel 2)
With an oscilloscope i measured the frequency on TP7 on the board, i have a square wave with 10ms period so the signal is OK.
Thanks
Philippe
- Labels:
-
STM32 Motor Control
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-06-27 6:33 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards