2025-01-01 11:56 PM
Does anybody know if control board NUCLEO-F446ZE and power board X-NUCLEO-IHM07M1 can be configured to support 2 motors (FOC) in STM32 MC Workbench?
2025-01-04 02:50 AM - edited 2025-01-04 02:59 AM
@apexyzdgme wrote:Does anybody know if control board NUCLEO-F446ZE and power board X-NUCLEO-IHM07M1 can be configured to support 2 motors (FOC) in STM32 MC Workbench?
Yes, the NUCLEO-F446ZE and X-NUCLEO-IHM07M1 can be configured to support two motors (FOC) in STM32 MC Workbench. You would need to set up two motor configurations in the MC Workbench and ensure proper wiring and power handling for both motors.