2021-07-27 11:48 AM
Hi everyone!
I try use SDK with sensor AS5600(12-Bit Programmable Contactless
Potentiometer) and 1/2-H Bridge Driver DRV8313
Motor is 24N28P
MCU: STM32F072C8T6
One shunt resistor with LM2904
I choose hall sensors in Workbench:
and I convert values AS5600 in HALL-values: 5,1,3,2,6,4 depends on angle. In my case every change of angle 4.25 degree - change hallstate in struct HALL_Handle_t
I do it in while() and if hallstate is changed I call void * HALL_TIMx_CC_IRQHandler( void * pHandleVoid ). Here and in static void HALL_Init_Electrical_Angle( HALL_Handle_t * pHandle ) I comment next code ih these functions:
/* pHandle->HallState =(uint8_t) ((LL_GPIO_IsInputPinSet( pHandle->H3Port, pHandle->H3Pin ) << 2)
| (LL_GPIO_IsInputPinSet( pHandle->H2Port, pHandle->H2Pin ) << 1)
| LL_GPIO_IsInputPinSet( pHandle->H1Port, pHandle->H1Pin ) );
*/
and instead of
bPrevHallState = pHandle->HallState;
i write
bPrevHallState = myVariableOfPrevHallState
But my motor don't spin - only vibrate or brake-on condition. It seems that I check out everything and have no idea what to do next.
Could you help me, please?
2021-08-04 9:42 PM
Dear @Shevtsov
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
2021-08-04 9:43 PM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards
2021-08-04 10:52 PM
Thank you for answer!
HW:
It's all on my PCB(I designed it).
SW:
2021-08-04 11:01 PM
I want to replace PCB that set in motor DM5015 and use my own pcb and control motor with CAN-interface.
And I need to use sensors like AS5600 - it needs to know position of rotor. My goal is make something like 6-axial mini-robot