2021-07-28 10:42 PM
Hi,
I have STEVAL-IPMNG8Q-3h and I want to drive PMSM motor.
In the code generated by the ST WORKBENCH, I get this error!!
"Description Resource Path Location Type
unknown type name 'RTC_HandleTypeDef'; did you mean 'I2C_HandleTypeDef'? stm32f3xx_hal_timebase_rtc_alarm_template.c /28.07/Drivers/STM32F3xx_HAL_Driver/Src line 98 C/C++ Problem"
How can I solve?
Have a good day.
2021-08-04 8:11 PM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards
2021-08-04 8:12 PM
Dear @Community member
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
2021-08-04 11:07 PM
Thank you for answer,
I want to drive PMSM 3-phase motor. So I have STEVAL-IPMNG8Q.
I have STM32F407G discovery board and STEVAL-IPMNG8Q. I want to drive the PMSM motor with my code but I'm having problems.
I'm using six-step control with timer CH1-CH1N pwm.The code I wrote is below.
int pwmSin[] = {0,18,20,30,40,50,60,70,80,90,80,70,60,50,40,30,20,0,0,18,20,30,40,50,60,70,80,90,80,70,60,50,40,30,20,0,0,18,20,30,40,50,60,70,80,90,80,70};
void motor_control(void) {
///--------- A HIGH- B LOW ---------///
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);
///--------- A HIGH- C LOW ---------///
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_3);
///--------- B HIGH- C LOW ---------///
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_3);
///--------- B HIGH- A LOW ---------///
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);
///--------- C HIGH- A LOW ---------///
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);
///--------- C HIGH- B LOW ---------///
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);
}
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
for( i = 0; i<64;i++){
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_1, pwmSin[i]);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_2, pwmSin[i]+16);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_3, pwmSin[i]+32);
motor_control();
if(i == 63){
i=0;
}
}
When I run this code the motor is locked. The motor could not move.
I know I need to generate a sine wave using pwm but something is wrong.
I was able to create a 120 degree angle difference between phases but I am getting a square wave output. I will be grateful if you could help me. I wish you good work.
2021-08-04 11:16 PM
I then used the STM Motor Control Workbench but the IGBT exploded. What could be my problem? How can I control STEVAL-IPMNG8Q?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.