cancel
Showing results for 
Search instead for 
Did you mean: 

Motor profiler fail in open loop test for my BLDC motor.

Slee.3
Associate II

Hi!

I am trying to profile the motor using B-G431B-ESC1 Discovery Kit.

But the motor barely moves in the electrical model. The most successful one from my test was done without any values in Max Speed and Max Current. It ran up to 320, 2000, 1500, 1000 RPM (4 times) but still couldn't finish the Electrical Model.

I tried with different values of Max Speed and Max Current. I have never finished the Electrical Model.

The motor has 4 pairs of poles, 3000RPM(Max), 30A (Max), and SM-PMSM.

Do you have any suggestion?

Regards,

Sangrae

1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards